CAP#.SOURCE
Description
Selects what will be captured on the trigger event. The captured value will be available with CAP#.P. The capture time CAP#.T is also captured for each trigger.
Examples
Usage
| Value | Description |
|---|---|
| 1 (default) | Position Feedback 1. FB1.P |
| 2 | Position Feedback 2. FB2.P |
| 3 | Position Feedback 3. FB3.P |
| 4 | Position Feedback 4. FB4.P |
| 5 | Position Feedback 5. FB5.P |
| 11 | Axis 1 Feedback. AXIS1.PL.FB |
| 12 | Axis 2 Feedback. AXIS2.PL.FB |
Not all drive model variants have the hardware to support all these options. For example, a single axis drive will not support option 12.
Context
See Capture.
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-00-00-000 |
General Information
|
Type |
Read/Write |
|
Units |
N/A |
|
Range |
1 to 5, 11 to 12 |
|
Default Value |
1 |
|
Data Type |
Integer |
| See Also | CAP#.P |
|
Stored in Non-Volatile Memory |
Yes |
Variants Supported
All variants are supported.
Industrial Ethernet Information
|
Command |
Index |
SubIndex |
Data Type |
Units |
Float Scale |
Access |
PDO Mappable |
|---|---|---|---|---|---|---|---|
|
CAP1.SOURCE |
4400h |
06h |
Unsigned8 |
- |
- |
Read/Write |
No |
|
CAP2.SOURCE |
4401h |
06h |
Unsigned8 |
- |
- |
Read/Write |
No |
|
ID |
Instance |
Attribute |
Name |
Data Type |
Access |
User Mappable |
|---|---|---|---|---|---|---|
|
31080 |
1 |
31080 (0x7968) |
CAP1.SOURCE |
Unsigned8 |
Read/Write |
Yes |
|
31081 |
1 |
31081 (0x7969) |
CAP2.SOURCE |
Unsigned8 |
Read/Write |
Yes |
|
Parameter |
PNU |
Data Type |
Access |
Units |
|---|---|---|---|---|
|
CAP1.SOURCE |
31080 |
Unsigned8 |
Read/Write |
- |
|
CAP2.SOURCE |
31081 |
Unsigned8 |
Read/Write |
- |
Related Topics